Dear Team,
I am using SN74AVC8T245PWR in a circuit. Same circuit is attached for your reference.
In one SN74AVC8T245PWR (Say IC1), Voltage across PIN 6 (A4) & PIN 11 (GND) is measured as 1V instead of 3.3V (Note the 3.3V pull up in the circuit attached).
So to confirm, I measured the voltage across same points in some other healthy ICs ((Say IC2 & IC3)). In it the voltage is measured as 3.3V.
This made me think, First IC ((Say IC1)) may be defective. I mean, that IC (PIN 6) sinks some amount of current (greater than ) from 3.3V pull up supply and due to this voltage across PIN 6 & GND may be lesser. Request you to confirm the same.
Also Pls let me know will the impedance at PIN 6 be same during power ON & power OFF conditions.I don't think both will be same. Because while measuring at power OFF condition in Healthy ICs (IC2 & IC3), Impedance across PIN 6 & GND is 4.7KOHM. I don't think same would maintain during power ON also. It should be around 1M during power ON. Right?
Thanks in Advance. Awaiting your reply.
Regards,
Devarajan R