This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV595A: Output Pulled Up to 3V3 While VCC = 0V

Part Number: SN74LV595A

Hi Logic Team,

My customer uses the LV595A with a pull up resistor at the outputs to keep the output an a known-state at all times (avoid Hi-Z). If VCC = 0V while the outputs are being pulled up, will I have a potential reverse leakage through the high side FET of the push-pull output? If so, how much current can the FET handle?

Related to this, when would I expect Hi-Z output? From what I understand, only when OE is pulled high. 

Thanks,

Leo