Other Parts Discussed in Thread: SN74LVC2G126, SN74LVC2G125, SN74HCS126, SN74HCS125, SN74LV125AT
Hi Experts,
We are looking for the logic buffer which has the same function of SN74LVC3G17 with OE control.
5V tolerant with 3.3V supply
3 channel
Ioff support ( even when Vcc is off, user can apply the voltage on the output pins(3.3V) )
OE support (when OE is inactive, output is Hi-Z.)
This is the logic to receive three input signals from an external board.
Regards,
Hisao Uchikoshi