Other Parts Discussed in Thread: SN74LV125A-Q1, SN74AHCT1G125-Q1, SN74AHC125-Q1
Hello team
I'm using TXB0104-Q1 for SPI communication with external flash.
I can see for the SPI clock signal that the signals are translated.
but for the MOSI part connected to B-1, I see a strange signal on A-1 (check figure 3 and 4 below)
VCCA = 3.2V
VCCB = 4.5V
SPI CLOCK B3
SPI CLOCK A-3
MOSI SIGNAL B-1
MOSI SIGNAL A-1