Dear Sir,
Is there any risk about this design. When the input signal voltage is 3.3V, the VCC of 74LVC1G07 is only 1.8V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
Is there any risk about this design. When the input signal voltage is 3.3V, the VCC of 74LVC1G07 is only 1.8V?
Dear Sir,
Thanks for you help!
The SN74LVC1G07 IC without positive clamp diode, so the voltage of input is 3.3V will not affecting the VCC(1.8V). So the design is OK. I'm right?
Thanks!
Hello,
Yes, that is correct. Since the input is overvoltage tolerant (without positive clamp diodes), it can be overdriven up to the VI (input voltage) recommended maximum specification without issue.
Best,
Michael
Dear Michale,
Worst case for logic low on MCU is 0,5V, minimum required input level on buffer(SN74LVC1G07) is 0,63 V (if buffer is supplied by 1,8 V), there is 0,1 V of margin. The question is how buffer will work during extreme temperature condition, on bigger population and during ALT test.
Thanks!