Other Parts Discussed in Thread: MSP432E401Y, SN74AHCT1G125
I am looking for a buffer IC with 1 or 2 gates (i.e. 1 bit or 2 bits) unlike the 4 bits of the SN54ACT244 which works of a 5V supply.
In addition I should be able to drive it from the output port pins of the TI MSP432E401Y launchpad which is a +3.3V device. The buffer output
should be rated at least +10mA and -10mA.
The SN54ACT244 has a logic input high and low of 2.0V and 0.8V which is perfect however it has a lot more internal buffers than i need.
Thanks
David Nyarko