Dear sir and madam.
In my design, I use TXS0108E to transfer the 1.8V Data Bus to 3.3 DataBus.
A side of TXS0108 is connected to 1.8V FPGA GPIO. And B side of TXS0108 is connected to 3.3V MRAM Data Bus.
The FPGA is XC7VX690T-2FFG1927. The MRAM is MR4A08BCYS35.
We meet the following problem.
Now we can write data from FPGA to the MRAM, but we can not read the data in MRAM.
By using a oscilloscope,We found out that the A side changes will result in the changes of B side. However,When the B side changes from 0 to 1, the A side always stay in zero.
We do not use the pull up resistor.