Other Parts Discussed in Thread: SN74AHCT1G32
Hi TI
There are tow questions that need to confirm.
1.When Vcc is 5V, the threshold is Vcc×0.7 or VM(Vcc/2) ?
If the input voltage is 3V, can it operate normally?
2.And why the TI solution VIH is around 3.5V(5V*0.7), but other vendor is around 2V-2.2V?