This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G07-EP: Clarification of output structure and logic state

Part Number: SN74LVC1G07-EP
Other Parts Discussed in Thread: SN74LVC1G07, SN74HCS72, SN74LVC1G06

Hi,

For this SN74LVC1G07-EP and the SNLVC1G06-EP the data sheets say open drain output and the logic diagram table use  H on the output instead of Hi-Z or Z in the data sheet of the non-EP versions.   Can you clarify the output structure of these logic devices?   Are there any more details to share regarding the H state on these devices in terms of usage?   Why is the data sheets done differently in the logic table; for instance are there any differences in the logical function or implementation on the board of the non-EP and EP versions?

Thank you,

HSG