This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC32T245: SN74AVCxT245 Maximum Data Rates Question

Part Number: SN74AVC32T245
Other Parts Discussed in Thread: SN74AVC16T245

Hi,

I would like to complete my design with TI's level shifter ICs, such as SN74AVC16T245 or SN74AVC32T245. In the datasheet, it says the IC supports maximum data rates at 380Mbps. I wonder this spec means SINGLE data in the bus or ALL.

Take SN74AVC32T245 for an example, if it means single data path, then the overall bandwidth is 380Mbps. If it means all data paths, then the overall bandwidth is 380Mbps x 32, which is nearly 12Gbps.

Hope I can get an accurate answer. Many thanks.