Other Parts Discussed in Thread: LSF0204-Q1
Hello,
does TXB0106-Q1 supports 100MHz translation like LSF0204-Q1?
I need a "Auto-Bidirectional Multi-Voltage Level Translator" for QSPI running with 85MHz clock.
Regards MW
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
does TXB0106-Q1 supports 100MHz translation like LSF0204-Q1?
I need a "Auto-Bidirectional Multi-Voltage Level Translator" for QSPI running with 85MHz clock.
Regards MW
Hey MW,
The best option for this would be the LSF0204-Q1. Its maximum data rate depends on the pull-up size and load capacitance. This training video goes into detail on this. VrefA can't be 3.3 V, but the pull-up voltage on the A port can be 3.3 V.