Hi support team.
Is there a time limit for the absolute maximum rated voltage?
My customer is experiencing -0.57V / + 4.15V undershoot and overshoot. Is there a problem with this condition?
The notes in the data sheet include the following:
> (2) The input and output negative-voltage ratings may be exceeded if the input and output current ratings are observed.
Is it the same on the positive voltage side?
Best regards,
Higa