This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC4T774: JTAG voltage level transceiver

Part Number: SN74AVC4T774
Other Parts Discussed in Thread: SN74AXC4T774, TXB0104, , TXB0108

Hello,

I need to convert the JTAG signals from 3.3V to 1.8V levels.

I thought of using the SN74AVC4T774RGYR.

Can this device do the job?

Is there any other device which can do this convertion?

Thnaks,

Asaf