Hello expert,
Could we know the difference between SN74AXC1T45DCK and SN74AVC1T45DCK? Do you have comparison table for these parts? Thanks a lot!
Best regards,
Ann Lien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello expert,
Could we know the difference between SN74AXC1T45DCK and SN74AVC1T45DCK? Do you have comparison table for these parts? Thanks a lot!
Best regards,
Ann Lien
Hey Ann,
The AXC and AVC are very similar families. Consider using the former (AXC) as it's faster with a wider supply range and has glitch-free power up.
Family | AXC | AVC |
Interface Support | Push-Pull | Push-Pull |
VCC (V) | 0.65 - 3.6 | 1.2 - 3.6 |
Drive Strength (mA) | 12 | 12 |
F_Max (MHz) | 190 | 190 |
Here's an app note on the AXC as well.
Glitch Free Power Sequencing With AXC Level Translators
Rami