Hi
The conversion between 1.8V and 5V CMOS levels, If the IC output is all push-pull structure, is the resistor Rpu necessary?
8-channel, what do you do with dangling channels?Do not connect?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The conversion between 1.8V and 5V CMOS levels, If the IC output is all push-pull structure, is the resistor Rpu necessary?
8-channel, what do you do with dangling channels?Do not connect?
Thanks!
Hey Neal,
The pullup isn't necessary if your application doesn't call for it. The image in the datasheet that you've shared is just showing many different ways to use the LSF0108-Q1 but you aren't limited to the setup shown. The LSF is a passive switch so if the architecture doesn't call for additional pullups outside of the normal pull ups your application would typically have (e.g. I2C).
For the LSF family you can leave unused pins floating:
[FAQ] What should be done with unused I/O pins of the level translator devices?
How many channels do you need? We do have a 4channel and 2 channel AEC-Q100 qualified versions in the in the family.
Thanks,
Rami
As this is shown in the datasheet, with 1.8V being up-translated to 5V, then yes - a pull-up resistor is absolutely necessary in that application. The LSF device cannot up-translate by itself (because it is a passive translator).
Please see this video: https://training.ti.com/translation-lsf-family-0?cu=1134826