Other Parts Discussed in Thread: SN74LXCH8T245
Hello,
I connect the following voltages to the part: VCCA = 3.3V, VCCB = 5V
Is it OK to apply at TTL signal (5V) to the A side of the device (with VCCA = 3.3V)?
The datasheet says that VIH Maximum = VCCI (3.3V), on the other hand the Absolute Maximum rating says 6.5V
Can it affect the operation / failure / damage?
Thanks a lot!
Max