Hello
Could you please recomend a latch or shift register to take and hold data from an MPS430 device sent to the control pins of a CD4066B device? The switch input is a low level audio source, the output is fed through a unity gain set op-amp opa890 With an expected 12V supply voltage for the CD4066B, the expected control pin low voltage is 2 volts, the expected high >7 volts. The difficulty I see is the shift registers I have so far looked at are all Vcc 5v max with proportionally lower values for 'high' and 'low'.
Ref. Pgs:
http://www.ti.com/product/cd4066b
http://www.ti.com/product/opa890
https://estore.ti.com/MSP-EXP430G2-MSP430-LaunchPad-Value-Line-Development-kit-P2031.aspx
I have looked at this but do not think it will work for me: http://www.ti.com/product/sn74lv595a-q1