Hi,
I just wonder if the SN74ABT125 outputs are push-pull?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I just wonder if the SN74ABT125 outputs are push-pull?
Yes the outputs are push pull.
Hi,
I had the chip SN74ABT125 connection as below:
Vcc = 5V
With OE = 0V and Vih = 3.3V, the output was measured @ 1.2V
Is the output supposed to be near Vcc when input is greater than 2V (according to its datasheet) ?