This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CD4504B not working when Vcc = 0V ??

Prodigy 90 points

Replies: 21

Views: 6113

Dear Experts,

I'm using a CD4504B level shifter to translate 5V signals to 12V.
However, the 5V power supply is not always present...
... and I have the impression that the device is doing stupid things (high power consumption, and output switching unexpectedly (at least it happened once...)).

Inputs are also not powered, but I have pull-downs on all the inputs, so I presume they should not disturb the CD4504B, but I can find no information about what is supposed to happen when VCC = 0 and VDD = 12V...

Does anyone know?

Thanks for your help!

  • Maybe my question is stupid, but there is no information in the data sheet... What are we supposed to do in this case?

  • In reply to Mike Info:

    Hi,

    The issues are wired. I take some samples to test it and will ask help from design team. When I get feedback I will let you know.

    The input is pulled down when VCC=0. Dose the pull-down resistor is used or connet input to ground directly?

    Thanks

     

  • In reply to Wei Lang:

    Hi,

    Thanks for your answer.

    All data inputs have a 20k resistor to ground. Vcc input has a capacitor to ground, and comes from a regulator that is powered down as well (sleep mode in my circuit, all power is cut except 12V).

    Best regards,

  • In reply to Mike Info:

    Hi,

    I built test circuits as below schematic.

    When VCC is powered at 5V and VDD is powered at 12V, all output ports are at low when input ports are pulled down by 20kohm resistor. The Icc current is less than 1mA and Idd current is about 5mA.

    When VCC is powered at 0V and VDD is powered at 12V, all output ports are at low when input ports are pulled down by 20kohm resistor too. The Idd current is about 1mA.

    In the test, there is no high current and output switching when VCC=0.

    The logic forum engineers are experts and more familiar with the CD4504B. They will give your answers.

    Thanks

    Wei

  • In reply to Wei Lang:

    There should not be any issues with Vcc at 0V and Vdd at 12V.  Be sure you inputs meet the rise and fall specs shon in the datasheet. If the inputs are too slow they can cause higher current ant the outputst to oscillate.

  • In reply to Wei Lang:

    Yes my circuit looks like this (except for the Select input which is tied to ground).

    What is surprising is that initially everything is fine. I have to wait something like 1.5 to 2 minutes until the problem occurs (power consumption of board going from 1 uA to 8 mA ! 8000 times higher !!!).

    Then I discovered that if I power up the 5V for a short time, the circuit is back to the micro-amp range.

    Really puzzling!

  • In reply to Mike Info:

    Is VCC tied directly to Vss?

  • In reply to Chris Cockrill:

    No. In fact Vcc comes from an LT3508 switching regulator, which is normally powered from Vdd.

    In deep sleep mode, there is a MOSFET switch that cuts off the Vdd input to the regulator, which in turn stops delivering the Vcc. There are some decoupling caps on Vcc, but I think that after more than 1 minute (when the problem occurs), they must be really empty!! 

    Measurement on Vcc show a little noise (in the millivolt range).

  • In reply to Mike Info:

    Vcc when shut off  it should be at 0V and not floated. The ESD/clamp protection diodes in the low side are tied to Vcc and  should not be floated. Also the switching threshold gets its reference form VCC and Vdd.

    You might try connecting Vcc to gnd when it is turned off ans see if that prevents the higher current that occurs after the part sits for a while.

  • In reply to Chris Cockrill:

    Well I've tried to manually shunt Vcc and gnd when in deep sleep mode to make sure the Vcc is exactly zero... but the problem still happens.

    What I observe is that :

    - before the high consumption, all outputs of the CD4504B are low = 0V

    - when the high consumption occurs, I see that the outputs swing from a few mV to 40 mV...

    - when I keep my voltmeter probe on an output, its voltage usually decreases to a few mV, when I switch and probe another output, then I see the same kind of behavior, which tends to indicate that the voltmeter internal resistance has an impact on the measurement... But it is not systematic, and sometimes I see voltage rising, then falling back. Behavior is really chaotic.

    The high consumption may come from the 4043B latch that is behind the CD4504B, when it sees non-null inputs.

    The question is: why are the outputs of the CD4504B not at 0V ???

    Vcc is now exactly 0V, inputs are all tied to GND through pull-downs, only Vdd is present...

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.