Hi,
I'd like to ask a question about this part: http://focus.ti.com/docs/prod/folders/print/sn74auc1g126.html
I'm operating it at 1.8V and it is buffering a 26MHz clock. I don't have tools to simulate the part using IBIS or anything like that and I'm just trying to figure out a few specs that don't seem clear in the datasheet. I'm wondering about the rise time and maximum capacitive loading capability.
I have a circuit that isn't passing the clock out very well as the long transmission line is having impedance and termination problems. There may also be some capacitance issues as one way I get the nice sine wave I need (AC coupling the output) is to place a 330pF cap in series and a 220pF cap to ground right after this buffer chip.
Thanks!