We are currently using the SN74LV08A with the following:
Vcc = 3.3V
1A (pin 1) = 3.3V
Can 1B (pin 2) safely be exposed to 5V given the above conditions?
If 1B is at 5V, will the output 1Y (pin 3) be 3.3V?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.