This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Buffer

Mastermind 8875 points

Replies: 1

Views: 461

Hello 

      Do we have a buffer IC that operation voltage =3.3V(both input and output voltage are 3.3V), the pin out separate two side of package like SN74AHC540

but without 3-state (enable function)?  Thank you.

BR

Patrick

  • Hi Patrick ,

    I can suggest SN74LVC3G34 which is 3 gate buffer without 3 state output .

    -Thanks,

    Shreyas

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.