In the LVC family of logic gates, can I use the output of a spare gate to reliably hold the unused inputs at a known level, or will it power up in an unknown and possibly unreliable state due to the linear/transition region? In other words, on a spare gate, can I connect its output to its inputs with a feedback resistor of 1-2 KOhms to prevent floating inputs? Will the output on power up be driven sufficiently low to hold the inputs at a steady low state, or will they potentially get stuck at an in between voltage level (not high or low)?
Thanks,
Josh