Hello all,
I'm using a SN74LV1T04 level shifter/inverter. The specification of ΔIcc in the datasheet is quite limited. It's only specified for 1.8V and 5.5V Vcc.
In my case Vcc varies between 2.5 and 3.6V. The input voltage is 0 or 1.8V. I would like some more detailed specification of ΔIcc as a function of Vcc and logic input levels.
My application needs to be very low power so ΔIcc is a critical parameter for me.
Is such information available?
Thanks,
Paul Beijer
--