Will I run into any problems if I pull the output up to 1.8V? (even though it is not open drain)
Vcc is 1.05V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Will I run into any problems if I pull the output up to 1.8V? (even though it is not open drain)
Vcc is 1.05V
Would you consider putting a blocking diode at the output of the device? You could (in essence) turn the device into an open-drain part by preventing the part from sourcing current (only allow sinking current, like an open-drain device). A schottky diode would add minimal delay and voltage drop.
This is incorrect, as Clemens pointed out. I have done this before with devices that don't have clamp diodes, but it won't work for this one - I should have thought it through a little more.
Emrys Maier said:Would you consider putting a blocking diode at the output of the device? … only allow sinking current
But sinking current from the higher voltage into VCC is the problem.
Now that I think more about it, that was a silly idea. Thanks Clemens.
Putting the diode at Vcc might do it though - prevent current backflow into the supply rail.