I am asking about how OE pins are connected.
As a typical application on the Datasheet, it is written that the OE pin is connected to Gnd by Pull Down resistor
1) So if I do not use 3-State mode, is it correct to connect OE pin to Vcca? Or what happens when I connect OE Pin to Vcca?
2) If I open the OE pin, can there be a problem in operation?
3)This may be a bit wide question, but when do I need to connect OE pins to Gnd?
4)Or is it appropriate for this device to use to connect OE pins to Gnd?
5)What are the advantages of using the three state mode as the typ application suggests?
Please help me~~!!
Thank you
Best regards