This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HCT374: Please provide the longetity , Temperature, speed, Density .

Part Number: CD74HCT374
Other Parts Discussed in Thread: SN74AHCT1G08, CD74ACT273, , CY54FCT273T

Dear all,

Please provide the longetity (availability of the product) , Temperature, speed, Density , pins and type of use(serial or Parallel) of below product list.

SN74AHCT1G08DBVR
CD74ACT273PWR
CD74HCT374M96

Regards.,

Dayananda Angadi.

  • Hi Dayananda,

    I'm not sure exactly what you're asking for, so I'm going to point you to a few resources that might help.

    First, our FAQ has a great deal of useful information, for example, the policy on obscolescence is available here:

    Thermal characteristics for parts are listed in their datasheets, which are available from the product folders here: SN74AHCT1G08, CD74ACT273, CD74HCT374

    If the datasheet is missing a particular value that you need, please let us know and I can look into it for you.

    The speed of devices is also a frequently asked question, the answer to which is located here: 

    I'm not sure what you mean by density -- are you talking about kg/m^3 or pin pitch (distance between pins)?  For the pin 'density' I would refer to the datasheet, and the other you'd have to measure.  That's not something we specify.

    For pins and type of use, that's all specified in the datasheets.

    Please let me know if something is confusing or difficult to find.

  • Thanks Emrys Maier.,


    Please provide alternate for below listed Memory IC which has been Obsolete.
    We are looking for Maximum Longetity (availability of the product) and Military Temperature(-55 to 125 C).
    Almost same pin configuration.

    a) IDT54FCT273ATDB octal latch
    (Integrated Device Technology )
  • Dayananda,
    This part number shows to be a direct replacement match.
    IDT part number TI generic # DLA SMD #
    IDT54FCT273ATDB CY54FCT273T 5962-9221503MRA

    If this answers your question, please click "Verify it as the answer"
    Regards,
    Wade