This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

SN74AHCT244: importance of the IC in the reference design of TIDA-00626

Intellectual 605 points

Replies: 1

Views: 241

Part Number: SN74AHCT244

respected,

 i have been working on the reference design of TIDA-00626. have developed the board. In BOM SN74AHCT244 was mentioned as U9. but in the datasheet of TIDA-00626 the SN74AHCT244 IC has not been placed. Should i place it or should i skip it. please let me know the same

  • Hi Pratik,
    It looks like they included the SN74AHCT244 to translate from 3.3V outputs on the MSP430 to the 5V inputs of another device.

    If you need to do a 3.3V signal up to 5V conversion, you will want to include a voltage translator (I would actually recommend using a dual supply translator like SN74LVC8T245 because it will reduce total power consumption)


    Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

    The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.