This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G06: Pull Up Resistor Design Guide

Part Number: SN74LVC2G06

Team,

Customer is looking at open drain type solution SN74LVC2G06 for 0Vin to 5.5Vout/ 3.3Vin to 0Vout. May I check with you any guideline for the chosen of pull up resistor?

Thanks.

Allan 

  • Hello Allan,

    Selecting a pull-up resistor is based on two primary concerns - speed and power.

    The smaller the pull-up resistor, the faster the edges will be, but the more power will be used.

    Larger pull-up resistors will use less power, but will result in slower edges.

    The equations that govern this are very basic:

    The power equation: P = IV

    Ohm's law: V = IR

    98% RC charge time: 4τ = 4RC

    Typically, engineers will use a pull-up resistor between 1kΩ and 10kΩ, but values are not limited to those.  If you get too small of a resistor, the current requirement can get too high for the device, and if you get too high of a resistor, the leakage current can start to become important.

    Two examples:

    A 1 Ω pull-up is obvously too small, as it would require 5A to operate at 5V

    A 10 MΩ pull-up is obviously too large, as even a 1 μA leakage current would cause a voltage drop of 10V.