This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHCT244: output current

Part Number: SN74AHCT244

We are trying to figure out if it would be acceptable to drive a MOSFET at a frequency of 20kHz using one of the output of a 74AHC244. We have captured the current waveforms during turn-on and turn-off, waveforms attached.

While the RMS is well within the Io spec. of table7 of the datasheet (“Limiting values”), the instantaneous current goes over the limit. I was wondering if the Io spec. refers to continuous current draw only or if it represent max. instantaneous current as well.

Would the following patterns present a reliability issue for the device if repeated continuously at a frequency of 20kHz.

Regards,

Doug