Hello
What is the recommend output current at Vcc=3.3?
The SN74LVC1G125-Q1 . SGES002C–APRIL 2003–REVISED APRIL 2008 datasheet (pg3) shows 16ma and 24ma for Vcc=3v.
The datasheet front page states "±24-mA Output Drive at 3.3 V".
To max reliability/thermals/life no doubt the lower current drive is better target. However whatis the impact of running at 20ma or 24ma ?
Seems as if 20ma would be comfortable?
Thanks & Regards