Other Parts Discussed in Thread: SN74AXC8T245
I have some questions about sn74gtl2003.
1. I want to translate from LVCMOS18(1.8V, Source of SN74GTL2003) ports to 3.3 LVTTL(3.3V, Drain of SN74GTL2003).
Is this possible? does SN74GTL2003 support LVCMOS18??
2. If I want to set LVCMOS18 ports as unidirectional input(Source of SN74GTL2003), do I have to connect pull-up resistors with 3.3V LVTTL ports(Output, Drain of SN74GTL2003))??
And also, upside down, If I want to set LVCMOS18 ports as unidirectional output(Source of SN74GTL2003), I do not need pull-up resistors with 3.3V LVTTL ports(Input, Drain of SN74GTL2003))??
Are these correct connection?