Dear SIR:
May I have question and double confirming regarding SN74LVC1G06 as below:.
According to SN74LVC1G06 spec. mention that " VCC MIN =1.65V ,MAX =5.5V ;
"When VCC = 1.65 V to 1.95 V ==>VIH MIN =0.65 × VCC ; VIL MAX =0.35 × VCC . "
" When VCC = VCC = 3 V to 3.6 V ==>VIH MIN =2V ; VIL MAX =0.8.V "
If we know the condition (A) "Input =1.8V =High ,0V=Low" ,base on above ,Is that meaning we need provide SN74LVC1G06's VCC =1.8V ,Right ?
Another condition (B) "Input =1.8V =High ,0V=Low" OR "Input =Unknow (Maybe=3.3V) =High ,0V=Low" ,base on above ,Is that meaning we still need provide SN74LVC1G06 VCC =1.8V ,Right ?
( Because If We provide SN74LVC1G06 VCC =3.3V ,When "Input =Unknow (Maybe=3.3V) =High ,0V=Low" will work ,but when "Input =1.8V =High ,0V=Low" SN74LVC1G06
will not work ,Right ? )
Figure as below: