Hi Team,
Customer wants to convert the 125Mhz clock signal from 1.2V to 1.8V, the datasheet says "Up to 500-Mbps Support When Translating from 1.8 to 3.3V". I think 125Mhz equals to 250Mbps.
Could you please help confirm if 125Mhz is supported on the EVM? The conditions are
1. VCCA is 1.2V, VCCB is 1.8V
2. the direction is A to B
3. 125Mhz is the input at A.
I know the data rate is related to the specific design. Can you share the scopeshot of the test on SN74AXC1T45EVM? Thank!
Best Regards,
Hao