This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4069UB: Absolute MAX of VIN on datasheet

Part Number: CD4069UB

Dear Technical Support Team,

The absolute MAX of VIN on datasheet shows 0.5V(MAX) and -0.5 to Vdd(MIN) below.

I think that this is typo and "Vdd+0.5V(MAX)" and -0.5(MIN) correctly.

If it is typo, could you fix it ?

Best Regards,

ttd