Other Parts Discussed in Thread: SN74LVC125A, SN74AHC125, CD74HC4050
Hello Logic Forum.
I am planning on using an SN74HC125 being fed with Vcc=3.3V, having its OE always 0. My question is: is it safe to have its inputs range from 0 to 5V, or would it be safer to use voltage dividers instead, to reduce the input voltage range from 0-5 to 0-3.3V?
If the latter were true: would the use of another similar device instead of the SN74HC125 make it possible not to use voltage dividers?
Thank you in advance, best regards.