This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] What are the power sequencing requirements for the translation device?

Mastermind 49850 points

Replies: 0

Views: 756

Click here for our parent FAQ

Some of the TI translators have requirements during normal operation mode to have Vcca <= Vccb ( TXS/ TXB) or Vrefb>= VrefA+0.8V(LSF). However, the TI translation devices do not specifically have any power sequencing requirements (power up and power down).

Usually, the datasheet’s power supply section mentions if there are any power sequencing recommendations. Note that the power sequencing can be modified according to the needs of the application/system without any performance or reliability concerns to the device.

In general, TI recommends having the ground connected before any supply is applied while the control and I/O ports are preferably at ground through weak pulldown resistors

Refer to the AXC app note which doesn’t require any power sequencing:

http://www.ti.com/lit/an/scea058a/scea058a.pdf

-Thanks,

Shreyas

Watch the Introduction to AXC Family

Read the app note on Glitch-free Power Sequencing for the AXC family

Evaluate the AXC8T245 EVM and watch the translation using the EVM