Other Parts Discussed in Thread: SN74LVC1T45, TLV3201
Hi
SN74LVC1G14(PN: 2600210008) is used by my customer.
They want to know the quiescent current when Vcc=5V, A=2.6V.
Thanks a lot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
SN74LVC1G14(PN: 2600210008) is used by my customer.
They want to know the quiescent current when Vcc=5V, A=2.6V.
Thanks a lot.
Hi Shawn,
Is there a reason why 2.6V is being used? The output is not guaranteed to switch at Vcc 5V and input at 2.6V.
The Icc can be very high in mA during this case and could cause reliability issues in the long run.
consider using a voltage level translator with Vcca at 2.5V and Vccb at 5.5V like SN74LVC1T45.