Hi,
I have some questions regarding the protection circuit (if there are any) for the little logic family:
- Question 1: Are there input protection diodes integrated in the SN74LVC components, to DGND and to VCC ?
- Question 2: Can we have the equivalent circuit of an SN74LVC component input port ?
- Question 3: Are there output protection diodes integrated in the SN74LVC components, to DGND and to VCC ?
- Question 4: Can we have the equivalent circuit of an SN74LVC component output port?
Thanks and regards
Annais