This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN74LV245A: SN74LV245A: Permissible input voltage at Vcc = 0V

Prodigy 160 points

Replies: 1

Views: 112

Part Number: SN74LV245A

Hi,team

Can this IC receive 5V at A1~A8 or B1~8 , even if the power is off?

thanks.

  • The absolute maximum ratings allow up to 7 V at the input pins, regardless of VCC.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.