This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ALVC125: SN74ALVC125

Part Number: SN74ALVC125

I'm going to use SN74ALVC125 connected to 1.8V VCC and inputs to 3.3V logic.

I see in app. notes that ALVC technology input is 5V tolerant but I don't see this specific note in SN74ALVC125 data sheet.

Just to be sure - is it tolerant to 3.3V when powered from 1.8V?

Regards,

Youry