I have a problem when using the buffer IC SN74LVC1G07. When the input signal speed is 500K, the output is normal. When the input signal speed is 2Mbps, the output waveform is seriously distorted and can not work properly. VCC is 2.5V .what's the reason? thanks!