This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G07: Apply SN74LVC1G07 in level shift application

Part Number: SN74LVC1G07
Other Parts Discussed in Thread: SN74LVC1G34

Dear E2E,

Could we use SN74LVC1G07 to operate in down translation from 3v3 to 1v8 application?

the input source is 3v3 as open drain type of driver and pullup through 300k to 3v3 and output is 1v8.

i think we need to use 1v8 as bias power voltage for SN74LVC1G07, but i am not sure if input voltage is higher than bias power pin. any concern?

in addition, what is the leakage current at input pin?

BR,

Jason