This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHCT244: Short time high output current

Genius 15770 points
Part Number: SN74AHCT244

Hello,

I have a question for SN74AHCT244 output current for capacitive load.

The datasheet(SCLS228M) defines absolute max of “Continuous output current, Vo<0 or Vo>Vcc)” as +-25mA.
But in my customer’s system, the peak output current is around +-78mA due to 0.01uF capacitance of RC filter while it is very short time.
The below is the circuit and waveform.



Does the customer have to keep this continuous output current, +-25mA, even if the time over 25mA is less than a few us like this figure?  
Does they need to adjust RC filter parameter to keep the peak current less than +-25mA?

Regards,
Oba