Hello team,
I would like to confirm about VT- value in Datasheet. In 6.5, VT-@Vcc5.5V is defined around 1.87V to 2.29V. However, in fig9 looks like VT- is around 0.5V to 1.0V.
Which is the correct value?
Thank you,
Kazuki Kitajima
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
I would like to confirm about VT- value in Datasheet. In 6.5, VT-@Vcc5.5V is defined around 1.87V to 2.29V. However, in fig9 looks like VT- is around 0.5V to 1.0V.
Which is the correct value?
Thank you,
Kazuki Kitajima
The datasheet says:
9.2.3 Application Curve
Figure 9 is created from the values given in the Electrical Characteristics. Linear interpolation shows the values between each given point.
The VT– values shown in the graph for 4.5/5.5 V are the same as ΔVT in 6.5, i.e., they were accidentally taken from the wrong line.
Hi Kazuki,
As clemens has mentioned Figure 9 is created from the values given in the Electrical Characteristics. I would trust the table in 6.5 for the value.
Vt- should be around 1.87V to 2.29V.
I will make a note to have Fig. 9 fixed when we do the next update to the datasheet.
Thanks!
-Karan