This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

SN74LV165A: We want to double check the device can be used with frequency below 45Mhz

Genius 10470 points

Replies: 1

Views: 72

Part Number: SN74LV165A

Hi team,

We want to double check the device can be used with frequency below 45Mhz, correct? Thanks.

  • Hi,

    Yes, this device can be used below 45MHz. The spec you are referring to is the fmax spec. The minimum Fmax value implies that this is the lowest maximum frequency we guarantee.

    Thanks!

    -Karan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.