Hi, I would like to verify the location of PIN 1 of SN74LVC2G07 chip. Based on the datasheet the PIN 1 is located at Q3. Am I right?
That means PIN 1 is at bottom most left of each pocket in the tape. Am I right?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I would like to verify the location of PIN 1 of SN74LVC2G07 chip. Based on the datasheet the PIN 1 is located at Q3. Am I right?
That means PIN 1 is at bottom most left of each pocket in the tape. Am I right?
Thanks
Thank you, Clemens.
It would be good if the datasheet drawing has the 'notch' as pin1 identifier to mimic the actual device. I gave the feedback, however, there could be some high running packages( eg DCK) which are manufactured in different regions with different pin1 identifier ( notch, dot , bar etc) for the same package.