This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74GTLPH16912: SN74GTLPH16912 this support BTL logic

Part Number: SN74GTLPH16912

Hi,

 I am using  SN74GTLPH16912 GTLP part design.

Can this part replace BTL transceivers because previous design using FB2030 part 5V compatible part.

New design using 3.3V logic peripheral planning to use this part.

On back plane side having BTL logic but this IC is GTLP , datasheet also not mentioned compatible with BTL.

Provide clarification on this part is compatible with BTL logic.

Regards,

Vinayak Arkachari