This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 54
Part Number: SN74LVC126A
I'm looking for a data buffer to handle a parallel video data bus running up to 300MHz at Vcc = 3.3V. Can anyone suggest a suitable device? Anything from 1 to 10-channel would do!
Thanks
300 MHz (= 600 Mbps) or 300 Mbps (= 150 MHz)?
In reply to Clemens Ladisch:
300MHz (we usually specify in this form for a parallel video bus)
In reply to Julian Hiorns:
There is no logic device rated for 600 Mbps.