Other Parts Discussed in Thread: 5-8-LOGIC-EVM
hi Team,
we have a SN74LVC2G07 return that has no output signal when input is applied
it's observed that the resistance measured from the Vcc to Vss is 6k, while the resistance measurement from a good IC is 21K~22K
may we check with the application, that what might the causing the failure? for example the input pins exceeds the abs max ratings -0.5V~6.5V
or current, temperature?
Thanks very much